DLPU048E August 2016 – July 2024
This command is used to read the host-specified values for the display image flip orientation. The default image flip settings are specified in the flash header file that is included along with the flash data.
Command Parameters
No command parameters.
Return Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:2 | Reserved |
1 | Short Axis Image Flip 0x0: Image not flipped 0x1: Image flipped | |
0 | Long Axis Image Flip 0x0: Image not flipped 0x1: Image flipped |