DLPU048E August 2016 – July 2024
The TPS99000-Q1 includes a watchdog that monitors a periodic pulse generated by the DLPC230-Q1 using a DLPC230-Q1 GPIO pin. This is used to confirm that the DLPC230-Q1 main application is functional. The main application configures the watchdog window during system initialization. If the pulse is not detected within the specified window, the TPS99000-Q1 will take action.