DLPU048E August 2016 – July 2024
This test monitors the DMD reset voltage levels each frame using TPS99000-Q1 ADC measurements. The following voltages are monitored:
If any of these voltages are measured outside of a specified maximum and minimum value, the test will take action. The allowable ranges are specified in the flash header file provided along with the flash binary file.