DLPU048E August 2016 – July 2024
The following table describes the error codes that may be received during main application execution. This preliminary list does not define every error code and will be updated during main application development.
CODE | NAME | DESCRIPTION |
---|---|---|
03 | Flash Out Of Range | Set during Flash Write command if the flash image is larger than 128Mb. |
04 | Flash Read Timeout | Set during startup if the flash device ID cannot be read. |
05 | Flash Busy | Set during any flash read, erase, or write operation if another operation is already accessing flash memory. |
06 - 09 | Internal Error | Internal system error. Contact TI for more information. |
10 | Invalid Command Type | Set if the next byte from the command interface is not the correct type. For example, if a data byte is read when an op-code byte is expected. This can occur if the host sends too many or too few bytes for a particular command. |
13 | Invalid Flash Write Sequence | Set during the flash write command if the flash has not been erased. |
15 | Invalid Command Op-Code | The requested command op-code does not exist. |
16 | Invalid Command Signature | Set if the signature bytes are invalid for the following commands: System Reset, Flash Erase, Clear Error History, or Clear Short Status. |
17 | Internal Error | Internal system error. Contact TI for more information. |
18 | Mismatch Command CRC / Checksum | A CRC or checksum in the command is invalid. |
19 | Mismatch Command Payload Size | The command payload size didn't match the number of bytes transmitted. |
20 | Internal Error | Internal system error. Contact TI for more information. |
22 | Software FIFO Full | The software command FIFO is full and cannot accept more commands. This error can be prevented by waiting for the System Busy Short Status bit to be set low between command transactions so that the FIFO does not overrun. |
26 | Flash Invalid Device | Set if the flash device is not found during startup, an unknown flash device is found during startup, a flash device is not found and a Flash Erase is requested,or a flash device is not found and a Flash Write command is requested. |
33 - 46 | Internal Error | Internal system error. Contact TI for more information. |
70 | Incorrect Command Header Format | The host command header format is invalid. |
71 | Read Activate Invalid CRC / Checksum | The host command had an invalid CRC or checksum during a Read Activate command. |
72 | Read Activate Header Early Termination | The host terminated a Read Activate transaction before the entire header data was sent. |
73 | Read Activate Response Early Termination | The host terminated a Read Activate transaction before the entire read payload was sent. |
74 | Read Activate Late Termination | The host terminated a Read Activate transaction later than expected based on the read payload length. |
75 | Read Activate Data Unavailable | Set if there is no read data available when the host sends a Read Activate command. |
76 | Host RX FIFO Overflow | A received host command caused the read FIFO to overflow, resulting in the loss of data from the previous read command. |
77 | Internal Error | Internal system error. Contact TI for more information. |
78 | Short Status Invalid CRC / Checksum | The host command had an invalid CRC or checksum during a Short Status command. |
79 | Short Status Header Early Termination | The host terminated a short status transaction before the entire short status header was sent. |
80 | Short Status Response Early Termination | The host terminated a short status transaction before the entire short status response was sent. |
81 | Short Status Late Termination | The host terminated a short status transaction later than expected. |
82 | Host TX FIFO Overflow | Software attempted to write to a full host interface FIFO. |
94 - 121 | Internal Error | Internal system error. Contact TI for more information. |
123 | Flash FIFO Timeout | Set during Flash Write command if software times out waiting for the serial flash controller. Also possibly set during startup if the serial flash controller times out while retrieving the flash device ID. |
125 - 128 | Internal Error | Internal system error. Contact TI for more information. |
129 | Invalid Read Prefetch Op Code | An invalid read op-code was sent using a Read Pre-Fetch command. |
139 | Command Error | Bezel horizontal offset exceeds -10% limit. |
140 | Command Error | Bezel horizontal offset exceeds +10% limit. |
141 | Command Error | Bezel vertical offset exceeds -50% limit. |
142 | Command Error | Bezel vertical offset exceeds +50% limit. |
143 - 147 | Internal Error | Internal system error. Contact TI for more information. |
148 | Command Error | Bezel horizontal offset is not a multiple of 2. |
149 | Command Error | Image orientation (flip) is invalid. |
150 - 153 | Internal Error | Internal system error. Contact TI for more information. |
154 | Fuse ID Error code | Number of lines * number of pixels exceeds the maximum resolution for this product |
157 - 161 | Internal Error | Internal system error. Contact TI for more information. |
162 | Command Error | Bezel vertical offset is not a multiple of 4. |
163 | Command Error | Execution delay error. |
164 | Command Error | GPIO invalid owner. |
165 | Command Error | GPIO wrong direction. |
166 | Command Error | Illumination Bin not found. |
167 | Command Error | System Mode not found. |
168 | Command Error | Contrast Parameter error. |
169 | Internal Error | Internal system error. Contact TI for more information. |
170 | Command Error | Flash invalid block type. |
171 | Command Error | Flash invalid block size. |
172 | Command Error | Flash invalid block version. |
173 | Command Error | Flash invalid data type. |
174 | Command Error | Invalid batch command. |
175 | Command Error | Batch command set invalid index. |
176 | Command Error | Flash invalid command sequence. |
177 | Command Error | Invalid payload length. |
179 | Command Error | ADC Measurement start or length parameter out of range. |
180 | Command Error | Command is not allowed in current operating mode. |
181 | Command Error | Temperature compensation source selection invalid. |
182 | Command Error | Reset is required after flash update. |
183 | Command Error | PWM duty cycle command parameter is greater than maximum allowed. |
184 | Command Error | De-gamma selection cannot be changed while illumination transition is in progress. |
185 - 200 | Internal Error | Internal system error. Contact TI for more information. |
201 | Command Error | Invalid source type selected. |
202 - 205 | Internal Error | Internal system error. Contact TI for more information. |
206 | Command Error | No splash screen at requested index. |
207 - 213 | Internal Error | Internal system error. Contact TI for more information. |
214 | Command Error | ASIC Device ID not yet available. |
215 | Command Error | System must stay in Standby mode until reset has occurred. |
216 | Command Error | ASIC Device ID invalid selection. |
217 | Command Error | Operating Mode Select invalid mode. |
218 | Command Error | Temperature compensation parameter invalid. |
219 | Internal Error | Internal system error. Contact TI for more information. |
220 | Command Error | DMD Memory BIST columns failed. |
221 | Command Error | DMD Memory BIST failed. |
222 | BIST Error | Loss of dimming / ping BIST failed. No dimming / ping command was received within the configured time frame. |
223 | Command Error | Start index for diagnostic memory is out of range. |
224 | Command Error | Number of bytes for diagnostic memory is out of range. |
229 | Command Error | External video checksum start column invalid. |
230 | Command Error | External video checksum number of pixels per line invalid. |
231 | Command Error | External video checksum start row invalid. |
232 | Command Error | External video checksum number of lines per frame invalid. |
233 | Command Error | No settings provided for external video checksum. Write External Video Checksum Settings command prior to enabling the test. |
234 | Internal Error | Internal system error. Contact TI for more information. |
237 | Internal Error | Internal system error. Contact TI for more information. |
238 | Command Error | Attempted to change external video checksum settings, but external video checksum is enabled. |
239 | Command Error | Average Picture Level command parameter is out of range. |
240 | Command Error | Command not available for this product type. |
241 | Command Error | TPS99000-Q1 RGB Limits parameter is out of range. |
242 | Command Error | TPS99000-Q1 TIA2 parameter error. |
244 | Command Error | Commanded periodic BIST is disabled by flash setting and cannot be enabled by host command. |
245 | Command Error | CMODE value out of range. |
246 | Command Error | Socket connectivity test is able to read DMD ID |
247 | Command Error | Reset required after empty socket test |
512 | BIST Error | Back End BIST 1 failed. |
513-516 | Internal Error | Internal system error. Contact TI for more information. |
517 | BIST Error | Diagnostics emergency shutdown. |
518 | Internal Error | Internal system error. Contact TI for more information. |
519 | BIST Error | Memory BIST 17 failed. |
520 | BIST Error | Memory BIST 18 failed. |
521 | BIST Error | Memory BIST 19 failed. |
522 | BIST Error | Memory BIST 20 failed. |
523 | BIST Error | Memory BIST 21 failed. |
524 | BIST Error | Front End BIST 1 failed. |
525 | BIST Error | Internal system error. Contact TI for more information. |
526 | BIST Error | Flash Table Transport CRC failed. |
527 | BIST Error | Internal system error. Contact TI for more information. |
528 | BIST Error | External video checksum control invalid. |
529 | BIST Error | Non-Periodic test invalid. |
530 | BIST Error | Memory BIST 1 failed. |
531 | BIST Error | Memory BIST 2 failed. |
532 | BIST Error | TPS99000-Q1 signal interface BIST failed. |
533 | BIST Error | Memory BIST 22 failed. |
534 | BIST Error | DLPC230-Q1 Command and Flash Interface Memory test failed. |
535 | BIST Error | External Video Checksum failed due to checksum mismatch. |
536 | BIST Error | Memory BIST 23 failed. |
537 | BIST Error | Memory BIST 24 failed. |
538 | BIST Error | Memory BIST 26 failed. |
539 | BIST Error | Memory BIST 25 failed. |
540 | BIST Error | Memory BIST 3 failed. |
541 | BIST Error | Memory BIST 12 failed. |
542 | BIST Error | Memory BIST 13 failed. |
543 | BIST Error | Memory BIST 14 failed. |
544 | BIST Error | Memory BIST 15 failed. |
545 | BIST Error | Memory BIST 16 failed. |
546 | BIST Error | Memory BIST 4 failed. |
547 | BIST Error | Memory BIST 5 failed. |
548 | BIST Error | Memory BIST 6 failed. |
549 | BIST Error | Memory BIST 7 failed. |
550 | BIST Error | Memory BIST 8 failed. |
551 | BIST Error | Memory BIST 9 failed. |
552 | BIST Error | Memory BIST 10 failed. |
553 | BIST Error | Memory BIST 11 failed. |
554 - 555 | Internal Error | Internal system error. Contact TI for more information. |
556 | DMD Training Error | DMD HS training failed: returned invalid results. |
557 | Internal Error | Internal system error. Contact TI for more information. |
558 | BIST Error | External video frame count out of sequence. |
559 | DMD Training Error | DMD HS Training failed: Insufficient DLL window. |
560 - 563 | Internal Error | Internal system error. Contact TI for more information. |
564 | DMD Compatibility Error | TPS99000-Q1 pixel type configuration is not compatible with the DMD used in the system. |
565 | DMD LS Error | Unexpected data was received during a transaction on the DMD low speed interface. |
566 | Flash Configuration Error | Invalid external video checksum fail action. |
567 - 572 | Internal Error | Internal system error. Contact TI for more information. |
573 | DMD Training Error | DMD HS training failed: real-time test controller HS training error 1. |
574 | DMD Training Error | DMD HS training failed: real-time test controller HS training error 2. |
575 | DMD Training Error | DMD HS training failed: real-time test controller HS training error 3. |
576 | DMD Training Error | DMD HS training failed: real-time test controller HS training processing error. |
577 | DMD LS Error | DMD Low Speed validation failed: processing error. |
578 - 586 | Internal Error | Internal system error. Contact TI for more information. |
587 | Flash Error | Serial flash device is locked. |
588 | System Mode Error | The currently selected system mode is not compatible with the source frame rate. |
589 | De-gamma Error | The requested de-gamma table was not found in the flash data. |
590 | Internal Error | Internal system error. Contact TI for more information. |
591 | ADC Error | An attempt to manually read an ADC channel measurement requested an invalid channel (-1). |
592 - 595 | Internal Error | Internal system error. Contact TI for more information. |
596 | ADC Error | ADC measurement error: retry count exceeded. |
597 | ADC Error | ADC interface communication error. Data, parity, or stop-bit error occurred during transaction. |
598 - 600 | Internal Error | Internal system error. Contact TI for more information. |
601 | ADC Error | Attempted to manually read ADC measurement, but channel selection was invalid (>=64). |
602 | ADC Error | ADC measurement error: value saturated at minimum or maximum. |
603 - 625 | Internal Error | Internal system error. Contact TI for more information. |
626 | TPS99000-Q1 Interface Error | TPS99000-Q1 parity error during read. |
627 | TPS99000-Q1 Interface Error | TPS99000-Q1 parity error during write. |
628 - 632 | Internal Error | Internal system error. Contact TI for more information. |
634 | Thread Monitor Error | Thread is non-responsive within timeout. |
636 | DMD Access Error | DMD low speed interface communication failed. The ASIC did not receive an ACK from the DMD. This can occur if there is a DMD connection issue, or if the flash low speed port configuration does not match hardware connections. |
637 - 652 | Internal Error | Internal system error. Contact TI for more information. |
653 | Flash Table Error | Flash Table Type 1 CRC failed. |
654 | Flash Table Error | Flash Table Type 2 CRC failed. |
655 | Flash Table Error | Flash Table Type 3 transport CRC failed. |
656 | Flash Table Error | Flash Table Type 3 CRC failed. |
657 | Flash Table Error | Flash Table Type 4 CRC failed. |
658 | Flash Table Error | Flash Table Type 5 memory access failed. |
659 | Flash Table Error | Flash Table Type 5 CRC failed. |
660 | Flash Table Error | Flash Table Type 6 memory CRC failed. |
661 | Flash Table Error | Flash Table Type 7 memory CRC failed. |
662 | Internal Error | Internal error. Contact TI for more information. |
663 | Flash Table Error | Flash Table Type 8 memory CRC failed. |
664 | Flash Table Error | Flash Table Type 9 memory access failed. |
665 | Source Error | External source measured active lines per frame does not match source definition. |
666 | Source Error | External source measured active pixels per line does not match source definition. |
667 - 668 | Internal Error | Internal system error. Contact TI for more information. |
669 | Source Error | External source Open LDI DLL could not lock to pixel clock. |
670 | Internal Error | Internal system error. Contact TI for more information. |
671 | Source Error | External source Open LDI port pixel clock frequency is not within the allowable range. |
672 | Source Error | External source Open LDI total pixels per line are unstable. |
673 | Internal Error | Internal system error. Contact TI for more information. |
674 | Source Error | External source parallel port pixel clock frequency is not within the allowable range. |
675 | Source Error | External source parallel port total pixels per line are unstable. |
676 | Source Error | External source pixel clock above the allowable range. |
677 | Source Error | External source pixel clock below the allowable range. |
678 | Source Error | External source VSYNC frequency greater than defined maximum. |
679 | Source Error | External source VSYNC frequency less than defined minimum. |
680 - 687 | Internal Error | Internal system error. Contact TI for more information. |
688 | Source Error | Source selected is invalid (not external source, test pattern, or splash screen). |
689 - 712 | Internal Error | Internal system error. Contact TI for more information. |
713 | Clock Configuration Error | Attempted to enable spread spectrum on the DMD interface, but the spread spectrum enable signal is configured to keep it disabled. |
714 - 733 | Internal Error | Internal system error. Contact TI for more information. |
734 | Clock Configuration Error | Attempted to enable spread spectrum on the clock generator, but the spread spectrum enable signal is configured to keep it disabled. |
735 - 742 | Internal Error | Internal system error. Contact TI for more information. |
743 | Flash Configuration Error | Flash structure version does not match the structure version required by the main application. |
744 | Flash Configuration Error | Flash block type is not supported. |
745 | Flash Configuration Error | Flash table address is outside of valid range. |
746 | Flash Configuration Error | Flash block does not exist. |
747 - 758 | Internal Error | Internal system error. Contact TI for more information. |
760 | BIST Error | Video frame counter failed to lock due to value out of range. |
761 | Internal Error | Internal system error. Contact TI for more information. |
762 | Flash Error | Flash data verification CRC failed. |
763 - 777 | Internal Error | Internal system error. Contact TI for more information. |
778 | GPIO Error | Invalid pin access. |
779 | GPIO Error | Invalid pin direction. |
780 | GPIO Error | Invalid polarity type. |
781 - 836 | Internal Error | Internal system error. Contact TI for more information. |
843 | System Voltage Error | System 1.1V rail out of range. |
844 | System Voltage Error | System 1.8V rail out of range. |
845 | System Voltage Error | System 3.3V rail out of range. |
846 | System Voltage Error | ADC external VREF voltage out of range. |
847 | System Voltage Error | DVDD voltage out of range. |
848 | System Voltage Error | LDOT_M8 voltage out of range. |
849 | System Voltage Error | VMAIN voltage out of range. |
850 - 868 | Internal Error | Internal system error. Contact TI for more information. |
869 | Temperature Error | The temperature sensor remote channel is open. This is determined by a bit read from the temperature sensor status. This could be caused by a faulty connection between the DMD temperature sensing diode and the temperature sensor. |
870-871 | Internal Error | Internal system error. Contact TI for more information. |
872 | Temperature Error | Temperature sensor not present. |
873 - 874 | Internal Error | Internal system error. Contact TI for more information. |
875 | Temperature Error | Errors occurred during temperature read. |
876 | Temperature Error | Unknown temperature sensor device. |
877 - 881 | Internal Error | Internal system error. Contact TI for more information. |
887 | ADC Error | TPS99000-Q1 ADC interface measurement read error: A TPS99000-Q1 Data Reception error, or an ADC command control timeline violation error, or a TPS99000-Q1 input all HIGH, or TPS99000-Q1 disabled error detected. |
888 | DMD Interface Error | Attempt to park the DMD failed. |
889 | DMD Interface Error | Attempt to unpark the DMD failed. |
890 | BIST Error | TPS99000-Q1 thermal conditions on chip have reached the warning level. If temperature continues to rise, system will reach die over-temp error temperature and emergency actions will be taken by TPS99000-Q1. |
891 | TPS99000-Q1 Interface Error | TPS99000-Q1 parity error on a main SPI port transaction occurred (command or write data) on previous command. |
892 | TPS99000-Q1 Error | TPS99000-Q1 top level state machine has changed states unexpectedly. Can be used to indicate to processor that TPS99000-Q1 has exited DISPLAY state due to a fault. |
893 | ADC Error | TPS99000-Q1 ADC error bit was set. This can occur due to ADC measurement saturation, measurement underflow, or parity errors on the ADC interface. |
894 | DMD Device ID Error | DMD device ID does not match flash project setting. |
895 | Temperature Error | Temperature is lower than the minimum DMD park temperature. |
896 | Temperature Error | Temperature is higher than the maximum DMD park temperature. |
897 | Internal Error | Internal system error. Contact TI for more information. |
898 | BIST Error | DMD clock out of range. |
899 | Internal Error | Internal system error. Contact TI for more information. |
900 | Temperature Error | DMD is parked and temperature function indicates that DMD is not allowed to unpark. |
901 | Flash Configuration Error | TPS99000-Q1 product ID does not match value in flash. Note that the product ID is different than the TPS99000-Q1 version number. |
908 - 910 | Internal Error | Internal system error. Contact TI for more information. |
911 | Flash Read Error | Attempted to read flash data, but the flash block has been erased. |
912 | Internal Error | Internal system error. Contact TI for more information. |
913 | Source Error | External source has been lost. This may occur as a result of source-lost monitoring, or may be triggered due to other external source test failures such as video checksums. |
914 | Source Error | External source has been lost and attempt to transition to alternate source failed. |
915 | BIST Error | Average Picture Level exceeded its specified limit. |
916 | Internal Error | Internal system error. Contact TI for more information. |
917 | BIST Error | Excessive brightness detector indicates an over-bright fault condition. |
918-919 | Internal Error | Internal system error. Contact TI for more information. |
920 | Command Error | TPS99000-Q1 illumination sync control setting is out of range. |
934 | Command Error | TPS99000-Q1 drive mode setting write parameter out of range. |
935 | Command Error | TPS99000-Q1 ADC configuration setting write parameter out of range. |
936 | Command Error | TPS99000-Q1 illumination sync control setting write parameter out of range. |
938 | BIST Error | TPS99000-Q1 checksum error in group 1 register set. |
939 | BIST Error | TPS99000-Q1 checksum error in group 2 register set. |
940 | BIST Error | TPS99000-Q1 checksum error in group 3 register set. |
941 | BIST Error | Either no ACK was received from DMD after sending requested transfer for DMD low-speed interface validation or a DMD register compare error was detected. |
942 - 945 | Internal Error | Internal system error. Contact TI for more information. |
946 | Source Error | Expected VSYNC signal did not arrive in the time allocated. |
947-948 | Internal Error | Internal system error. Contact TI for more information. |
949 | BIST Error | DMD VRESET voltage reading is out of range. |
950 | BIST Error | DMD VOFFSET voltage reading is out of range. |
951 | BIST Error | DMD VBIAS voltage reading is out of range. |
952 | ADC Error | Sequence aborted so the ADC measurement data could not be read. |
953 | Source Error | The flash data defining the source to be displayed when the external source is lost contains invalid settings (test pattern, splash, system mode, or VSYNC frequency). |
954 | BIST Error | Multi-bit ECC memory error detected. |
955 | BIST Error | Single-bit ECC memory error detected. |
956 - 960 | Internal Error | Internal system error. Contact TI for more information. |
961 | BIST Error | Sequence clock ratio is not within the specified limits. |
962 - 966 | Internal Error | Internal system error. Contact TI for more information. |
967 | BIST Error | DMD reset instruction watchdog error. |
968 | BIST Error | Sequencer instruction watchdog error. |
969 | BIST Error | Frame memory buffer swap watchdog error. |
970 - 971 | Internal Error | Internal system error. Contact TI for more information. |
972 | BIST Error | Register CRC mismatched. |
973 - 974 | Internal Error | Internal system error. Contact TI for more information. |
983 - 999 | Internal Error | Internal system error. Contact TI for more information. |
1000 | Source Error | Vertical blanking error. Most likely caused by insufficient vertical front porch. |
1001 - 1006 | Internal Error | Internal system error. Contact TI for more information. |
1007 | BIST Error | DMD low speed interface parity error. |
1008 | System Voltage Error | ADC external bandgap voltage out of range. |
1009 - 1010 | Internal Error | Internal system error. Contact TI for more information. |
1011 | BIST Error | TPS99000-Q1 watchdog 1 did not detect a rising edge within the expected trigger window. |
1012 | BIST Error | TPS99000-Q1 watchdog 2 did not detect a rising edge within the expected trigger window. |
1013 - 1014 | Internal Error | Internal system error. Contact TI for more information. |
1015 | System Voltage Error | Driver power voltage is out of range. |
1016 | Internal Error | Internal system error. Contact TI for more information. |
1017 - 1022 | Internal Error | Internal system error. Contact TI for more information. |
1023 | Internal Error | Splash thread has terminated on an error. |
1024 - 1025 | Internal Error | Internal system error. Contact TI for more information. |
1026 | Flash Configuration Error | TPS99000-Q1 version does not match value in flash. |
1027 - 1067 | Internal Error | Internal system error. Contact TI for more information. |
1068 | Command Error | Diagnostic memory interface received an invalid command |
1069 | Command Error | Excessive brightness BIST cannot be command because the functionality is set to internal mode in flash |
1070 | BIST Error | DAC ADC Loop BIST: Current Control DAC error |
1071 | BIST Error | DAC ADC Loop BIST: Photo Feedback DAC error |
1072 | BIST Error | DAC ADC Loop BIST: Overbright DAC error |
1073 | Internal Error | Internal system error. Contact TI for more information. |
1077 - 1078 | Internal Error | Internal system error. Contact TI for more information. |
1079 | BIST Error | The provided current limit percentage threshold was not within 0-100. |
1080 | BIST Error | Photo feedback BIST failed. |
1081 | TPS99000-Q1 Interface Error | TPS99000-Q1 SPI transaction detected a read of swapped bytes. |
1082 | Internal Error | Internal system error. Contact TI for more information. |
1083 | PWM Temperature management error | DMD and PWM Temp management are both enabled and are using the same PWM GPIO |
1084 | PWM Temperature management error | PWM Temperature management duty cycle setting is outside range of 0-100%. Verify LUT in the flash is correct. |
1085 | PWM Temperature management error | PWM Temperature mangement output selection invalid. |
1086 | PWM Temperature management error | PWM Temperature management temperature source invalid. Please refer to Section 8.2.33 |
1087 | PWM Temperature management error | PWM Temperature failed to set PWM output. |
2011 - 2043 | Internal Error | Internal system error. Contact TI for more information. |