DLPU048E August 2016 – July 2024
The HOST_IRQ signal is an interrupt from the DLPC230-Q1 that is used to notify the host that a serious system error has occurred. This would generally result in an emergency shutdown. The HOST_IRQ signal will be set HIGH in this situation. Additional information on emergency shutdown can be found in Section 6.2.