DLPU048E August 2016 – July 2024
This command is used to read back the host-specified values for the loss-of-ping-command function.
Command Parameters
No command parameters.
Return Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:0 | Timeout length Maximum allowed time in milliseconds between ping command transmissions. 0 = Disable |