DLPU057A March 2018 – April 2022 DLP3030-Q1
The Extra Information field is a part of the configuration file that can be used to store any information in the form of 32 bit key-value pairs. For example, the key 0xB217D12F is mapped to the address in the Piccolo where the ASIC Build Information is stored. This SPI command is used to get the corresponding key for a given index. An input of ‘0’ returns the number of keys, any other index will cause the piccolo to return Key [index - 1].