DLPU057A March 2018 – April 2022 DLP3030-Q1
This is the data response for a valid request to read the Generic Command List type. The type is returned in the form of ASCII values of each character one by one from the start to the end of the string.
Byte | Description |
1 | Response Byte (01h) |
2 | Length (1Fh) |
3 - 33 | ASCII Value of Each Character of the Command List Type (from first to last) |
34 | Checksum (Sum of bytes 1 to 33) |