DLPU057A March 2018 – April 2022 DLP3030-Q1
This command can be used to park or un-park the DMD. If the Park byte = 1, the DMD is parked. If the Park byte = 0, the DMD is un-parked.
Byte | Description |
1 | Command Byte (04h) |
2 | Length (01h) |
3 | Park |
4 | Checksum (Sum of bytes 1 to 3) |