DLPU057A March 2018 – April 2022 DLP3030-Q1
This command requests a read of the PWM Sensitivity. PWM sensitivity is the minimum change in PWM input for each LED that can ensure one fine (HRPWM) pulse change in the corresponding output pulse width.
Byte | Description |
1 | Command Byte (6Fh) |
2 | Length (00h) |
3 | Checksum (6Fh) |