DLPU057A March 2018 – April 2022 DLP3030-Q1
This command is used to set the sensor gain. This command is available only in the calibration mode (see Section 3.35 to enable calibration mode).
Byte | Description |
1 | Command Byte (D2h) |
2 | Length (01h) |
3 | Sensor Gain |
4 | Checksum (Sum of bytes 1 to 3) |
The sensor gain can only have values ‘0’, ‘1’, ‘2’ and ‘3’ as it is an input to the two select bits of a 4 to 1 Mux. The actual gain applied is hardware dependent and is stored in the calibration file. It can be obtained by using the Sensor Gain Map as described in Section 3.42.