DLPU057A March 2018 – April 2022 DLP3030-Q1
This command gets the voltages of the 1.2-V, 1.8-V, 2.5-V and 3.3-V rails. For this command to work correctly these rails must be connected to ADC Inputs A0, B3, B6 and B7 respectively. The command also returns if the system has not been brought out of reset due to one or more of the power rail voltages being out of tolerance. If voltage monitoring is enabled, the Piccolo SW regularly measures the power rail voltages. In this case, the command reads the last measured voltage. When voltage monitoring is disabled, this command triggers ADC conversions to poll the voltage on the four rails.