DLPU057A March 2018 – April 2022 DLP3030-Q1
This command programs the binary data starting from the location next to the last programmed location. The length of binary data should be multiple of 2 ranging from 2 bytes to 254 bytes. Also, it checks if the command is trying to program beyond the region specified by the Start Address and Length settings before programming the data.
Byte | Description |
1 | Command Byte (F6h) |
2 | Length (3 to 255) |
3 | Secondary Op-code – Program (02h) |
4 to 257 | Binary Flash Data |
258 | Checksum (Sum of bytes 1 to 257) |
Note: Length (byte 2) is number of write bytes. Its value should be number of bytes of binary flash data + 1.