DLPU072C June 2018 – January 2024 DLPC3434
Table 3-34 describes the write parameters.
Parameter Bytes | Description |
---|---|
Byte 1 | Batch file number |
MSB | Byte 1 | LSB | |||||
---|---|---|---|---|---|---|---|
b7 | b6 | b5 | b4 | b3 | b2 | b1 | b0 |
Bit | Type | Description |
---|---|---|
7-1 | R | Reserved |
0 | W | 3-D Reference 0h = Next Frame Left 1h = Next Frame Right |
The 3-D Reference is used to specify whether a frame of data contains left eye data or right eye data. The 3-D reference is provided to the display as either a GPIO hardware signal or through sending this command. The selection is made using the Write 3-D Control command. When using this command as the reference, it is recommended that the command be sent every frame, or at the minimum, at the start of each eye pair. For example, the command can be sent before each left eye frame. At a minimum, it must be sent once at the start of 3-D operation. If the 3-D Reference is misaligned with the data, it can be corrected using this command or by using the Polarity of 3-D Reference parameter in the Write 3-D Control (20h) command.
When the Write 3-D Reference command is received, its parameter value will be applied to the image data following the next VSYNC or Start of Frame command.
When this command is received, software must set up the internal 3-D reference generator. If the command is sent every frame, software will ensure that the output of the internal 3-D reference generator remains accurate.