DLPU072C June 2018 – January 2024 DLPC3434
This command specifies the actuator orientation value. The command input value represents 1 of the 24 possible combinations in which 4 subframes can be ordered. Internally, the input is further modified by the current image orientation. Therefore, the input maps to 4 different subframe orderings.