DLPU101D December   2020  – July 2024 DLPC900

 

  1.   1
  2.   Trademarks
  3.   Read This First
  4. About This Guide
  5. Related Documentation from Texas Instruments
  6. If You Need Assistance
  7. DLP LightCrafter Single DLPC900 EVM Overview
    1. 4.1 Welcome
    2. 4.2 DLP LightCrafter Single DLPC900 Evaluation Module (EVM) Hardware
    3. 4.3 EVM Board
    4. 4.4 Other Items Needed for Operation
    5. 4.5 DLP LightCrafter Single DLPC900 Connections
      1. 4.5.1 DLP LightCrafter Single DLPC900 LED Enable and PWM Outputs
      2. 4.5.2 DLP LightCrafter Single DLPC900 Trigger Input and Output Voltage Selectors
    6. 4.6 DLP LightCrafter Single DLPC900 EVM Flex Cable
    7. 4.7 DLP LightCrafter Single DLPC900 EVM and DMD EVM Assembly
  8. Quick Start
    1. 5.1 Power-up the DLP LightCrafter Single DLPC900 EVM
    2. 5.2 Creating a Simple Pattern Sequence
  9. Operating the DLP LightCrafter Single DLPC900 EVM
    1. 6.1  DLP LightCrafter Single DLPC900 Control Software
    2. 6.2  PC Software
    3. 6.3  System Common Controls
      1. 6.3.1 Operating Mode
      2. 6.3.2 Connected DMD Type
      3. 6.3.3 EVM Information
      4. 6.3.4 Status
    4. 6.4  System Settings
    5. 6.5  Video Mode
      1. 6.5.1 Video Support
    6. 6.6  Pattern Modes
      1. 6.6.1 Menu Bar
      2. 6.6.2 Creating a Pattern Sequence in Pattern On-The-Fly Mode
      3. 6.6.3 Creating a Pattern Sequence in Pre-Stored Pattern Mode
      4. 6.6.4 Reordering a Pattern Sequence using the Edit LUT Feature
        1. 6.6.4.1 Special Considerations for Input Triggers when using the Edit LUT Feature
      5. 6.6.5 Creating a Pattern Sequence in Video Pattern Mode
      6. 6.6.6 Creating a Pattern Sequence With DMD Block Load
      7. 6.6.7 Pattern Settings
    7. 6.7  Batch Files
      1. 6.7.1 Execute Batch File
      2. 6.7.2 Creating and Saving Batch Files
        1. 6.7.2.1 Creating and Saving a Batch File Using the GUI
        2. 6.7.2.2 Creating a Batch File Using a Text Editor
      3. 6.7.3 Loading a Batch File
      4. 6.7.4 Adding a Batch File to the Firmware
    8. 6.8  Peripherals
      1. 6.8.1 Peripherals Tab
      2. 6.8.2 Debug Tab
    9. 6.9  Firmware
      1. 6.9.1 Adding or Removing Patterns from the Firmware
        1. 6.9.1.1 Deleting Images
        2. 6.9.1.2 Adding Images
        3. 6.9.1.3 Adding Both Images and Batch Files
      2. 6.9.2 Reprogram Firmware for a Different Supported DMD
    10. 6.10 Flash Device Parameters
    11. 6.11 JTAG Flash Programming
    12. 6.12 Programming an EDID
  10. Connectors
    1. 7.1  Input Trigger Connectors
    2. 7.2  Output Trigger Connectors
    3. 7.3  DLPC900 UART
    4. 7.4  DLPC900 I2C Port 0
    5. 7.5  DLPC900 I2C Port 1
    6. 7.6  DLPC900 I2C Port 2
    7. 7.7  JTAG Boundary Scan
    8. 7.8  GPIO and PWM
    9. 7.9  Power
    10. 7.10 External Parallel Video Connector
  11. Power Supply Requirements
    1. 8.1 External Power Supply Requirements
  12. Safety
    1. 9.1 Caution Labels
  13. 10Revision History

Creating a Pattern Sequence in Video Pattern Mode

Creating a Video Pattern Mode sequence is also similar to Pattern On-The-Fly Mode. The difference is that the patterns are streamed from the input video source. The user must create the video images and then input them through the RGB parallel interface. The input video source vertical sync is used as the triggering mechanism. The input video source must be stable and locked and continuously being applied, otherwise the firmware detects that the source was lost and a solid curtain is displayed. While the video source is stable and locked, the status box for Locked to External Source remains checked.

Follow these steps to create a Video Pattern Mode sequence.

  1. Make sure the EVM is powered up and operating correctly, and the Connected radio-button is lit green.
  2. Select Video Mode from the Operating Mode group box, and then select the HDMI radio-button from the IT6535 Receiver group box and finally click the Set button. (Select the DisplayPort radio-button if using this input connector). The Locked to External Source status box is checked after a few seconds.
  3. Verify the video source is displayed. If no video source is displayed, then make sure the PC or host is supplying the correct resolution and frame rate. See Video Support for video support.
  4. Select Video Pattern Mode from the Operating Mode group box, and then click the Pattern Design button so that the large black panel is displayed as shown in Figure 6-6.
  5. Click the Add Pattern button on the Menu bar and add 3 patterns. (Hover over buttons in the Menu bar to see the tool tip).
  6. Click the Select All Patterns button to select all images.
  7. Set exposure time to 1215µs and dark time to 0µs.
  8. Select the first image and select a bit depth of 2, start bit G0, and color Green.
  9. Select the second image and select a bit depth of 4, start bit R0, and color Red.
  10. Select the third image and select a bit depth of 3, start bit B0, and color Blue
  11. Click the Select All Patterns button.
  12. Remove the check from the Frame Change box.
  13. Select pattern 0 (first pattern) only and check the Frame Change box.
  14. Click the Update LUT button.
  15. Click the Start button to run the sequence. The system displays a green 2-bit sequence based on G0 - G1 for 1215μs, a red 4-bit sequence based on R0 - R3 for 1215μs, and a blue 3-bit sequence based on B0 - B2 for 1215μs with the remainder of the video frame time dark. This sequence repeats every frame with the new video data for that frame.
  16. Click the Stop button to end this example.

See Figure 6-14 after all settings have been applied.

DLPC900 Video
                    Pattern Mode Figure 6-14 Video Pattern Mode