DLPU101D December 2020 – July 2024 DLPC900
Creating a Pre-Stored Pattern sequence is very similar to Pattern On-The-Fly Mode. The difference is that the patterns are pre-stored in flash memory.
If images are not present in the flash memory, then proceed to Section 6.9.1 to add the images to the firmware and upload them to the EVM, then return here for steps on creating the pattern sequence.
To start creating a Pre-Stored Pattern sequence, follow the steps in Section 6.6.2 with the only change in step 2. In step 2, select the Pre-Stored Patten radio-button and then proceed with step 3.