DLPU101D December 2020 – July 2024 DLPC900
Click the Firmware button to display the Firmware panel as shown in Figure 6-23. In this panel a user can update the firmware with patterns, batch files, and set start-up conditions.
Before uploading firmware, verify the EVM is powered-up, operating as expected and connection has been established with the GUI. To update the firmware on the EVM click the Browse button and locate the firmware file for the EVM type. Then click the Upload button.
Beginning with GUI 5.3 the user can choose to either:
By default the Bootloader Area is skipped, but unchecking the Skip Bootloader Area box causes the Bootloader to be reloaded. Use this option with caution.
Within the Power up Defaults group box, a user can select the default power-up state by checking the Startup State check box and then selecting the state from the drop-down list box.
If the IT6535 digital receiver is present on the hardware, then the user can enable the use of this receiver by checking the HDMI/DP Receiver check-box.
A Debug Mask check box was added in GUI 5.3. Check this box to have the debug mask specified in the entry box executed on power up. Copy the string from the Debug Mask shown in the Debugging Trace box of the Debug Mode tab in Section 6.8.2.
If a default batch file is needed, then see the Batch File section in this guide.
The DLPC900 can also be controlled over the I2C interface on I2C port 0. The default DLPC900 secondary address is 0x34. This address is programmable using the I2C secondary address within the Power up Defaults group box.
The GUI permits the user to perform a bus swap on the DMD by checking the DMD Bus Swap box and selecting between Channels A and B. This feature is a firmware configuration option that only takes effect after uploading the firmware onto the EVM. However, when using the DLP LightCrafter Dual DLPC900 EVM the user can perform a bus swap on both the primary and the secondary by selecting each check box per desired channel.
The GUI also permits the user to enable Spread Spectrum Clock Generator Support. The user can select from .5%, .75%, or 1% in the drop down menu. This option uses internally controlled clock spreading to help minimize EMI due to high-speed signals. More information on the spread spectrum feature and DMD bus swapping can be found in the DLPC900 data sheet.