DLPU102C December 2020 – July 2024
The Edit LUT feature is only available in Pre-Stored Pattern Mode and Pattern On-The-Fly Mode when using GUI 4.0 or later in conjunction with Firmware 5.0 or later. This feature allows the user to manipulate the pattern display sequence without having to reload or change any data in the DLPC900 memory. The Edit LUT button appears on the right hand side of the Pattern Mode tab after adding patterns as described in Section 4.6.2.
The LUT Editor panel is shown in Figure 4-12 where the column labeled SNO (for example, Sequence Number) represents the pattern display slot numbers according to the order set (after clicking Update LUT) in the Pattern Design tab as shown in Figure 4-11. The user can then reorder those patterns by either manually entering the pattern number of the choice into a row in the LUT entry column or loading a text file beginning with the word Reorder followed by the desired numerical pattern slots as shown in Figure 4-13.
The following steps detail an example using the Edit LUT feature with five patterns in Pattern On-The-Fly-Mode:
When using the GUI interface, each pattern carries several items of information corresponding to the slot that was inserted in the original LUT order. Therefore, when reordering a pattern to a different slot in the LUT, the LUT retains the original assigned bit information, timing (exposure and dark time), LED color, and trigger information and not the information that is located in the reassigned slot in the LUT. For example, if pattern 3 contains a trigger input to begin the user’s execution in Figure 4-11 and is reordered to slot 2 as shown in Figure 4-12, then the trigger input is now located at slot 3 in the LUT rather than slot 0.
In Pre-Stored Pattern Mode, reordering the LUT does not change the pattern locations as the LUT does in Pattern On-The-Fly Mode. Only the requested bit information, timing, color, and trigger information are reordered based on the user’s updated LUT. However, a possibility to manipulate the pattern information after reordering the sequence by manually editing the batch file commands uploaded to the EVM rather than using the GUI.
An important note is to understand the Edit LUT feature by giving names to the patterns, as shown above the patterns in Figure 4-11, and treating them as the batting order in a baseball game. This way, to picture the distinction between the slot order numbers is easier in the SNO column (the new batting order) and the patterns that are inserted into the LUT Entry column (the batters). For example, Bob retains his batting statistics independent of his batting position (for example, bit information, timing, color, trigger), so if he originally bats first (slot 0 in Figure 4-11) but is moved to fifth in the new batting order (reorder LUT entry 4 in Figure 4-12) he retains all of his properties. The only difference is that now he does not bat (for example, is not displayed) until after the four batters (patterns) preceding him (Sue, Joe, Matt, and Sam). Notice also that in our example Joe bats twice in the new batting order (SNO 2 and 5). There is only one Joe, who bats twice in the new batting order. In the same way, a pattern in the original pattern list can be displayed in many positions in the reordered display LUT, without adding or removing any patterns in DLPC900 memory. Therefore, in terms of the system memory, the memory is only changed when using the Update LUT feature but never when using the Edit LUT (Reorder) feature in the Figure 4-11.