DLPU102C December 2020 – July 2024
Upon execution of the DLP LightCrafter DLPC900 GUI application, the panel shown in Figure 4-1 is displayed. The GUI panel contains the following three sections:
In any of the GUI sections, clicking a Get button reads the current settings of that particular subsection. Clicking the Set button programs the settings into the respective subsection. Note that some commands can require additional steps before the GUI display is updated.