DLPU107 May 2022 DLP5532-Q1
A diagram of all connections is shown in Figure 2-1.
For correct orientation of the numbering of leads notice that on the SPI cable there is a notch at the top. Note that there is some unused cables from the FTDI cable and unconnected pins on the SPI cable.
It is also possible to communicate with the EVM through I2C. Note that there is some unused cables from the FTDI cable and unused cables from the I2C cable.
The following provide visual references for the fan cable connections involving the DLP5532PROJHBQ1EVM projector itself.
The following provide visual references for the LED cable connections involving the DLP5532PROJHBQ1EVM projector itself.
Please do not attempt to remove the four screws on the LED heat sinks as this impacts the alignment of the illumination system.