To update the firmware, use the
following steps:
- Download the latest flash image
for your EVM from TI.com.
- Go to the Backup Firmware page in
the Firmware section of the EVM GUI to create a backup of the existing firmware
as a flash image file.
- Click the browse button to select
the file name and location of the backup flash image file and click the Start
Backup button.
- After a successful backup, go to
the Update Firmware page in the Firmware section of the EVM GUI to program the
latest flash image file.
- Click the browse button to select
the flash image file and then click the Start Update button.