DLPU124 june 2023
The DLPLCRC910EVM is a flexible evaluation module which, when coupled to one of the supported DLP DMD EVMs and an APPS FPGA board enables the sending of customer created patterns to the DLPC910 Controller, and then to the attached DMD for display. The DLP LightCrafter DLPC910 EVM and the supported DMD EVMs are offered for purchase separately so that customers can determine which elements customers wish to piece together for an application evaluation system.
The following items are not included with the EVM and need to be purchased separately if needed for customer evaluation: