DLPU134 April   2024

 

  1.   1
  2.   Trademarks
  3. 1Purpose and Scope
  4. 2UART Host Interface
    1. 2.1 UART Requirements
    2. 2.2 UART Commands
    3. 2.3 UART Read Commands
    4. 2.4 UART Command Builder Tool
  5. 3MicroSD Card Playback
    1. 3.1 MicroSD Card Overview
    2. 3.2 MicroSD Card Formatting and Configuration
    3. 3.3 MicroSD Card Playback Operation
  6. 4Graphics Library
    1. 4.1 Graphics Library Overview
    2. 4.2 Initial Animations
    3. 4.3 MicroSD Card Images
    4. 4.4 Splash Image
    5. 4.5 Smart Home Demo
  7. 5DSI Mode
    1. 5.1 DSI Mode Overview
  8. 6Revision History

Splash Image

The MSPM0 demo supports the ability to display the splash images that are stored inside of the DLPC3421 controller on the EVM.

Starting from the main menu GUI, the user can select the flash image option. Once a long press is registered the MSPM0 will enter statement St_MMENUFLASH. This case statement will create a button select animation, change input source select, and display the splash image . The function will iteratively select the splash images and display them to the user. When this process is finished there will be a message with instructions on the display. Follow those to get back to the main menu.