JAJSCD1B June 2016 – March 2019 TPS63070
PRODUCTION DATA.
The VSEL pin allows to dynamically select between two different output voltages on the adjustable version. The voltage is set by a resistor that is connected between the FB and the FB2 pin. FB2 is connected to GND if VSEL = high. FB2 is high impedance if VSEL= low. The transition speed during a voltage change is defined by the loop bandwidth of the device and can be adjusted by adding a feed-forward capacitor in parallel to R1.
The resistor values for the feedback divider and FB2 are in the 50-500kΩ range. R3 is calculated as follows:
For more details on how to use VSEL see Technote SLVAE62.