JAJSCS0C December 2016 – January 2018 TPS22810
PRODUCTION DATA.
The VIN to VOUT voltage drop in the device is determined by the RON of the device and the load current. The RON of the device depends upon the VIN conditions of the device. Refer to the RON specification of the device in the Electrical Characteristics table of this datasheet. Once the RON of the device is determined based upon the VIN conditions, use Equation 8 to calculate the VIN to VOUT voltage drop.
where
An appropriate ILOAD must be chosen such that the IMAX specification of the device is not violated.