JAJSCX6B January 2017 – July 2019 LMK04610
PRODUCTION DATA.
Given a remote radio head (RRU) type application which needs to clock some ADCs, DACs, FPGA, SERDES, and an LO. The input clock is a recovered clock which needs jitter cleaning. The FPGA clock should have a clock output on power up. A summary of clock input and output requirements are as follows:
Clock Input:
Clock Outputs:
It is also desirable to have the holdover feature engage if the recovered clock reference is ever lost. The following information reviews the steps to produce this design.
If JESD204B support is also required for the clock outputs, see JEDEC JESD204B for more details.