JAJSCX6B January 2017 – July 2019 LMK04610
PRODUCTION DATA.
PLL2 has four input modes which can be selected by the user. These modes give more flexibility to adjust the PLL2 bandwidth. See Table 16.
INPUT MODE | DESCRIPTION |
---|---|
Doubler Mode | The Input clock gets multiplied by 2. The duty cycle of the clock is <50%. |
Doubler invert mode | This mode is same like the doubler mode, where the input clock gets multiplied by 2, but the duty cycle of the output clock is >50%. |
Pulse mode | The duty cycle of the input clock is adjusted to a fixed value and is >50%. |
RDIV mode | The input divider is used to divide down the frequency with the range as shown in Table 15. |