JAJSDR6C August 2017 – February 2022 TIC12400-Q1
PRODUCTION DATA
Each switch input can be programmed to enable or disable interrupt generation upon status change by configuring registers INT_EN_COMP1 to INT_EN_COMP2 (for comparator inputs) and INT_EN_CFG1 to INT_EN_CFG4 (for ADC inputs). Interrupt generation condition can be adjusted for THRES_COM (for IN0-IN11) by adjusting the IN_COM_EN bit in the MATRIX register.
The abovementioned registers can also be used to control interrupt generation condition based on the following settings:
Note interrupt generation from switch status change is disabled for all inputs by default upon device reset.