8.5.1.1 Programming Sequence
When the device is first powered up, it must be initialized, and the ordering of this programming is important. The sequence is listed below. After this sequence is completed, the device should be running and locked to the proper frequency.
- Apply power to the device and ensure all the supply pins are at the proper levels.
- If CE is low, pull it high.
- Wait 500 µs for the internal LDOs to become stable.
- Ensure that a valid reference clock is applied to the OSCin pins.
- Program register R0 with RESET = 1. This will ensure all the registers are reset to their default values. This bit is self-clearing.
- Program in sequence registers R125, R124, R123, ..., R1 and then R0.