JAJSER5A February 2018 – April 2018 LMK05028
PRODUCTION DATA.
The PDN pin (active low) can be used for device power-down and used to initialize the POR sequence. When PDN is pulled low, the entire device is powered down and the serial interface is disabled. When PDN is pulled high, the device POR sequence is triggered to begin the device start-up sequence and normal operation as depicted in Figure 64. If the PDN pin is toggled to issue a momentary hard reset, the negative pulse applied to the PDN pin should be greater than 200 ns to be captured by the internal digital system clock.
PDN PIN STATE | DEVICE OPERATION |
---|---|
0 | Device is disabled |
1 | Normal operation |