JAJSES9 February 2018 DAC8771
PRODUCTION DATA.
Figure 123 illustrates a simplified block diagram of the voltage output stages of the DAC8771.
When designing for a shared voltage and current output terminal it is important to consider leakage paths that may corrupt the voltage or current output stages.
When the voltage output is active and the current output is inactive the IOUT pin becomes a high-impedance node and therefore does not significantly load the voltage output in a way that would degrade VOUT performance. When the voltage output is inactive and the current output is active switches S1, S2, and S4 all become open while switch S3 is controlled by the POC bit in the Reset Config Register. When the POC bit is set to a 0, the default value, switch S3 is closed when VOUT is disabled. This creates a leakage path with respect to the current output when the terminals are shared which will create a load dependent error. In order to reduce this error the POC bit can be set to a 1 which opens switch S3, effectively making the VOUT pin high-impedance and reducing the magnitude of leakage current.