JAJSEV0G july 2016 – august 2023 DP83822H , DP83822HF , DP83822I , DP83822IF
PRODUCTION DATA
PCS Loopback occurs in the PCS layer of the PHY. No signal processing is performed when using PCS Loopback.
PCS Input Loopback is enabled by setting bit[0] in the BISCR.
PCS Output Loopback is enabled by setting bit[1] in the BISCR.