JAJSF69A April 2018 – October 2018 ADS112C04
PRODUCTION DATA.
Up to 16 ADS112C04 devices can be connected to a single I2C bus by using different address pin configurations for each device. Use the address pins, A0 and A1, to set the ADS112C04 to one of 16 different I2C addresses. Figure 69 shows an example with three ADS112C04 devices on the same I2C bus. One set of pullup resistors is required per bus line. If needed, decrease the pullup resistor values to compensate for the additional bus capacitance presented by multiple devices and increased line length.