JAJSFF8E October 2012 – May 2018 BQ27545-G1
PRODUCTION DATA.
0x2e SOH percentage: this read-only function returns an unsigned integer value, expressed as a percentage of the ratio of predicted FCC(25°C, SOH Load I) over the DesignCapacity(). The FCC(25°C, SOH Load I) is the calculated full charge capacity at 25°C and the SOH current rate which is specified by SOH Load I. The range of the returned SOH percentage is 0x00 to 0x64, indicating 0 to 100% correspondingly.