JAJSFF8E October 2012 – May 2018 BQ27545-G1
PRODUCTION DATA.
As the name suggests, the bq27545-G1 secure-memory authentication key is stored in the secure memory of the bq27545-G1. If a secure-memory key has been established, only this key can be used for authentication challenges (the programmable data flash key is not available). The selected key can only be established/programmed by special arrangements with TI, using the TI’s Secure B-to-B Protocol. The secure-memory key can never be changed or read from the bq27545-G1.