JAJSFR0B July 2018 – October 2019 TPS563231
PRODUCTION DATA.
The output voltage is set with a resistor divider from the output node to the FB pin. 1% tolerance or better divider resistors are recommended. Start by using Equation 2 to calculate VOUT.
To improve efficiency at very light loads consider using larger value resistors, too high of resistance will be more susceptible to noise and voltage errors from the FB input current will be more noticeable.
Choose the value of RFBB to be 10 kΩ. With the desired output voltage set to 3.3 V and the VREF = 0.6 V, the RFBT value can then be calculated using Equation 2. The formula yields to a value 45.3 kΩ of RFBT.