JAJSG99 September 2018 ADS1235
PRODUCTION DATA.
The modulator is an inherently stable, fourth-order, 2 + 2 pipelined ΔΣ modulator. The modulator samples the analog input voltage at a high sample rate (fMOD = fCLK / 8) and converts the analog input to a ones-density bit-stream with the density given by the ratio of the input signal to the reference voltage. The modulator shapes the noise of the converter to high frequency, where the noise is removed by the digital filter.