JAJSGH2B November 2017 – September 2022 ADS7142-Q1
PRODUCTION DATA
In this mode, the ADC can be configured to store up to 16 conversion results in the data buffer based on user command. In this mode, the user can either start or stop the burst of data as described in the following two sections.