JAJSH94 April 2019 BQ79606A-Q1
PRODUCTION DATA.
The CRC check is done on all of the registers in the OTP space (as indicated in the Register Summary table). The register values are concatenated together with the lowest addressed register as the first data byte and the highest addressed register as the last data byte used in the CRC calculation. Using the same bit ordering as described in Calculating Frame CRC Value calculate the CRC on that number in the same manner and with the same polynomial as described in Calculating Frame CRC Value.