JAJSHK4E March 2015 – August 2021 TPS65982
PRODUCTION DATA
The SPI controller provides a serial interface to an external flash memory. The recommended memory is the W25Q80DV 8 Mbit Serial Flash Memory. A memory of at least 2 Mbit is required when the TPS65982 is using the memory in an unshared manner. A memory of at least 8 Mbit is required when the TPS65982 is using the memory in an shared manner. See the Section 9.5.1 section for more information.