JAJSJA2A October 2020 – August 2024 TPS99000S-Q1
PRODUCTION DATA
The current limit of the LM3409 is determined by the current draw of the IADJ pin of the TPS99000S-Q1, which is controlled by an internal DAC and an external resistor connected to the R_IADJ pin of the TPS99000S-Q1. The approximate peak current limit can be calculated using the following equation:
Where: