JAJSJF5C April 2021 – November 2024 DP83TC812R-Q1 , DP83TC812S-Q1
PRODUCTION DATA
To read a register in the extended register set and automatically increment the address register to the next higher value following the read operation:
Instruction | Example: Read register 0x0170 & 0x0171 |
---|---|
1. Write the value 0x001F (address function field = 00, DEVAD = 31) to register REGCR. |
Write register 0x0D to value 0x001F |
2. Write the desired register address to register ADDAR. |
Write register 0x0E to value 0x0170 |
3. Write the value 0x801F (data, post increment on reads and writes function field = 10, DEVAD = 31) to register REGCR. | Write register 0x0D to value 0x801F |
4. Read the content of the desired extended register set register to register ADDAR. | Read register 0x0E |
5. Subsequent reads to register ADDAR (step 4) reads the next higher addressed data register selected by the value of the address register; the address register is incremented after each access. | Read register 0x0E |
Step 4 Reads register 0x0170 and because post increment is enabled, Step 5 reads register 0x0171.