JAJSJK9B December 2021 – May 2024 TMAG5328
PRODUCTION DATA
The TMAG5328 BOP is set by connecting a resistor or a voltage source to the “ADJ” pin. Figure 7-1 shows how to use resistor R1 to set the BOP. Figure 7-2 shows hows to use a DAC as a voltage source for setting the BOP. Using the DAC allows the user to dynamically change the BOP with software. To use a DAC, the output of the DAC must settle within 4µs after the 80µA current source of the “ADJ” pin is turned ON.
As a DAC alternative, Figure 7-3 shows how a voltage divider can be used as a voltage source. In Figure 7-3, an operational amplifier is placed between the voltage divider and the “ADJ” pin so that the voltage fed to the “ADJ” pin is not impacted by the internal current source of the TMAG5328 when the current source is turned ON. To use an op amp, the output of the op amp must settle within 4µs after the 80µA current source of the “ADJ” pin is turned ON.
A potentiometer or rheostat can be integrated into a voltage divider, and the user can adjust this potentiometer to dynamically update the BOP. Figure 7-4 shows how to use a potentiometer in a voltage divider to set the BOP of the TMAG5328. The maximum output voltage, which determines the maximum BOP, is set based on the values of resistors R1 and R3. The minimum output voltage, which determines the minimum BOP, is set based on the values of the maximum potentiometer resistance, R1 resistance, and R3 resistance. Select a minimum output voltage greater than 0.16V and a maximum output voltage less than 1.2V.
Figure 7-5 shows how the TMAG5328’s internal current source can drive a potentiometer or rheostat instead of a voltage divider. In this implementation, make sure the resistor R2 is at least 2kΩ to ensure that the “ADJ” resistance is always above the minimum 2kΩ. The sum of the maximum potentiometer resistance and the resistance of R1 must also be less than 15kΩ.
Multiple TMAG5328 devices can be used in the same system. When setting the BOP using a resistor, TI recommends that each TMAG5328 has a “ADJ” resistor, even if multiple TMAG5328 devices have the same “ADJ” resistor value. Figure 7-6 shows an example implementation that has three TMAG5328 devices. If each device is set to the same BOP, then the resistances of R1, R2, and R3 are equal.
When setting the BOP using a DAC, one DAC can be used to set the “ADJ” pin voltage of multiple devices only if the output of the DAC can sink the current from all of the TMAG5328 devices. Figure 7-7 shows an example of a DAC driving the “ADJ” pin of three TMAG5328 devices. A DAC can only work reliably in this specific scenario if the output of the DAC can settle within 4µs after being exposed to the three “ADJ” current sources. Each current source is 80µA, therefore the DAC can only reliably work if the output of the DAC can settle within 4µs after being exposed to 80 x 3 = 240µA of current.