JAJSKH6A April 2022 – May 2024 TUSB1004
PRODUCTION DATA
A typical usage of the TUSB1004 device is shown in Figure 7-2. The device can be configured either through its GPIO pins (SSEQ[1:0] and CEQ[1:0] pins) or through its I2C interface. In the example shown below, the TUSB1004 is configured in pin-strap mode with adaptive EQ (AEQ) enabled. The MODE pin is pulldown to GND through a 1-kΩ resistor. The AEQENZ is pulldown to GND which will enable AEQ for CRX1 and CRX2 receivers. Because AEQ is enabled, CEQ[1:0] pins can be left floating. The SSEQ[1:0] in this example is also floating but they need to configured to match the loss of the pre-channel (XAB).