JAJSKK6A November 2020 – December 2021 TPS7H4010-SEP
PRODUCTION DATA
The TPS7H4010-SEP is internally compensated. Typically, select RFBT ≤ 100 kΩ, then CFF is not needed. When very low quiescent current is needed, RFBT = 1 MΩ may be used. If COUT is mainly ceramic type low ESR capacitors, an external feed-forward capacitor CFF may be needed to improve the phase margin. Add CFF in parallel with RFBT. CFF is chosen such that the phase boost is maximized at the estimated crossover frequency fX. Equation 21 was tested.
With this design, because RFBT = 100 kΩ is selected, no CFF is needed.