JAJSLC9A February 2021 – August 2021 TCA9416
PRODUCTION DATA
The TCA9416 has an OE input that is used to disable the device by setting OE low, which prevents any signals from propagating across the device. This pin is referenced to the VCCA supply. The rise and fall time accelerators are also disabled. Note that the internal pull up resistors will still be enabled if the supply is above VUVLO. The disable time (tdis) indicates the delay between the time when OE goes low and when the outputs are disabled (Hi-Z). The enable time (ten) indicates the amount of time the user must allow for the one-shot circuitry to become operational after OE is taken high.