JAJSLE6C July 2020 – July 2024 TMUX6234
PRODUCTION DATA
Off isolation is defined as the ratio of the signal at the drain pin (D) of the device when a signal is applied to the source pin (Sx) of an off-channel. Figure 6-10 shows the setup used to measure, and the equation used to calculate off isolation.