JAJSLQ9C February 2016 – August 2021 TPS65981
PRODUCTION DATA
The ADC voltage inputs are each divided down to the full-scale input of 1.2 V. The ADC current sensing elements are not divided.
Table 9-6 lists the divider ratios for each ADC input. The table also shows which inputs are auto-sequenced in the round-robin automatic readout mode. The C_CC1 and C_CC2 pin voltages each have two conversions values. The divide-by-5 (CCn_BY5) conversion is intended for use when the C_CCn pin is configured as VCONN output and the divide-by-2 (CCn_BY2) conversion is intended for use when C_CCn pin is configured as the CC data pin.
CHANNEL # | SIGNAL | TYPE | AUTO-SEQUENCED | DIVIDER RATIO | BUFFERED |
---|---|---|---|---|---|
0 | Thermal Sense | Temperature | Yes | N/A | No |
1 | VBUS | Voltage | Yes | 25 | No |
2 | SENSEP | Voltage | Yes | 25 | No |
3 | IPP_EXT | Current | Yes | N/A | No |
4 | PP_HV | Voltage | Yes | 25 | No |
5 | IPP_HV | Current | Yes | N/A | No |
6 | PP_5V0 | Voltage | Yes | 5 | No |
7 | IPP_5V0 | Current | Yes | N/A | No |
8 | CC1_BY5 | Voltage | Yes | 5 | Yes |
9 | IPP_CABLE | Current | Yes | N/A | No |
10 | CC2_BY5 | Voltage | Yes | 5 | Yes |
11 | GPIO5 | Voltage | No | 1 | No |
12 | CC1_BY2 | Voltage | No | 2 | Yes |
13 | CC2_BY2 | Voltage | No | 2 | Yes |
14 | PP_CABLE | Voltage | No | 5 | No |
15 | VIN_3V3 | Voltage | No | 3 | No |
16 | VRSTZ_3V3 | Voltage | No | 3 | No |
17 | BC_ID | Voltage | No | 3 | Yes |
18 | LDO_1V8A | Voltage | No | 2 | No |
19 | LDO_1V8D | Voltage | No | 2 | No |
20 | LDO_3V3 | Voltage | No | 3 | No |
21 | Unused | Voltage | No | 3 | Yes |
22 | GPIO0 | Voltage | No | 3 | Yes |
23 | Unused | Voltage | No | 3 | Yes |
24 | GPIO2 | Voltage | No | 3 | Yes |
25 | GPIO3 | Voltage | No | 3 | Yes |
26 | GPIO4 | Voltage | No | 3 | Yes |
27 | GPIO5 | Voltage | No | 3 | Yes |
28 | GPIO6 | Voltage | No | 3 | Yes |
29 | GPIO7 | Voltage | No | 3 | Yes |
30 | GPIO8 | Voltage | No | 3 | Yes |
31 | BUSPOWERZ | Voltage | No | 3 | Yes |