JAJSLQ9C February 2016 – August 2021 TPS65981
PRODUCTION DATA
Placement of components on the top and bottom layers is used for this example to minimize solution size. The TPS65981 is placed on the top layer of the board and the majority of the components are placed on the bottom layer. When placing the components on the bottom layer, place them directly under the TPS65981 in a manner where the pads of the components are not directly under the void on the top layer. Figure 12-3 and Figure 12-4 show the placement in 2-D. Figure 12-5 and Figure 12-6 show the placement in 3-D.